System overview
A typical FactoryTalk Updater installation is multiple FactoryTalk Updater Agents
with a single FactoryTalk Updater Server and FactoryTalk Updater Client. FactoryTalk Updater
Agent, FactoryTalk Updater Client, and FactoryTalk Updater Server machines must be in the same
domain.
Typical FactoryTalk Updater system

FactoryTalk Updater Agent
FactoryTalk Updater Agent collects information and activation license data from the
Rockwell Automation software installed on the computer. Install the FactoryTalk Updater
Agent on each computer that requires data collection. FactoryTalk Updater Agent is installed
by default with most Rockwell Automation software. FactoryTalk Updater Agents collect and
store software inventory, activation data and activation transactions to a local database.
The FactoryTalk Updater Agents update the FactoryTalk Updater Server database once a minute
if there have been any changes since the last transmittal. If the connection between
FactoryTalk Updater Agent and FactoryTalk Updater Server is lost, the FactoryTalk Updater
Agent database buffers and persists data locally. When the connection is reestablished, the
FactoryTalk Updater Agent transmits all the new data to the FactoryTalk Updater Server.
FactoryTalk Updater Server
FactoryTalk Updater Server communicates with online FactoryTalk Updater Agents to receive
collected data and saves it to the FactoryTalk Updater Server database. To avoid issues,
limit FactoryTalk Updater Server installations to one instance per intranet with a maximum
of 100 connected FactoryTalk Updater Agents. FactoryTalk Updater Server connects to the
Product Compatibility and Download Center to retrieve the latest software information. A
user sign-in from FactoryTalk Updater Client is not required for FactoryTalk Updater
communication to PCDC. FactoryTalk Updater uses its own Rockwell certification to
authenticate with PCDC.
FactoryTalk Updater Client
FactoryTalk Updater Client displays information collected by the FactoryTalk Updater
Server. The FactoryTalk Updater Client presents most information visually. Export data to a
.csv file. Some large data sets, such as Add On Profiles, are not displayed on the screen
and require an Export to a .csv file. Monthly rollup patch deployment requires an
administrator to sign in to the FactoryTalk Updater Server and PCDC.
Provide Feedback