FactoryTalk Updater command-line parameters
Parameter | Description |
---|---|
/? | Displays the usage options for parameters. |
/ExportInventory=”value” | Exports the inventory information from all online agents. Specify the value of an
existing directory path or the full path for the file to export. The file to export
must be a .csv file. |
/ExportActivation=”value” | Exports activation information from all online agents. Specify the value of an
existing directory path or the full path for the file to export. The file to export
must be a .csv file. |
/ExportLog=”value” | Exports the log information from the client. Specify the value of an existing
directory path or the full path for the file to export. The file to export must be a
.csv file. |
/ExportAop=”value” | Exports Add-On Profile (AOP) information from all online agents to local. You can
specify the value of an existing directory path or the full path for the file to
export. The file to export must be a .csv file. If the value is a directory, it must
exist. |
/ExportCompatibility="value" | Exports product compatibility issues from all online agents to a comma-separated
value (CSV) file. |
/DownloadPath=”value” | Specifies the download path of the client. The value of this parameter must be an
existing directory path. |
/CheckInterval=”value” | Specifies the interval schedule for the automatic scanning of all machines. Set
this parameter to a value between 1 and 366 days. |
/AddAgents | Adds agents to the server by a single IP address or by a range of addresses.
Specify agents in this format: /AddAgents=”10.108.1.1,10.224.1.1-10.224.1.100” |
/AgentUserName | Uses the administrator's username of the target agents. |
/AgentPassword | Uses the administrator's password of the target agents. |
/Group | Specifies a group name when adding agents to the server. |
/UserName | Specifies the username used to connect to the server. |
/Password | Specifies the password used to connect to the server. |
Examples
The following example shows how to use the command-line parameters to export information:
CommandPrompt.exe /ExportInventory="C:\InventoryInfo\InventoryInfo.csv" /ExportActivation="C:\ActivationInfo\Activations.csv" /ExportLog="C:\ClientLog\Log.csv" /ExportAop="C:\AopInfo\Aop.csv" /ExportCompatibility="C:\CompatibilityIssuesFolder\CompatibilityIssues.csv" /UserName="user" /Password="password"
The following example shows how to use the command-line parameters to add agents and specify a group name:
CommandPrompt.exe /AddAgents="10.108.1.1,10.224.1.1-10.224.1.100" /AgentUserName="admin" /AgentPassword="admin" /Group="groupA" /UserName="user" /Password="password"
Provide Feedback