Export lists of machines, activations, AOPs, and logs

Export lists of machines, activations, Add-On Profiles (AOPs), and logs as .csv files. Save the files to a local or network drive.
  1. From the main menu, select
    Export
    , and then select
    Machines
    ,
    Activations
    ,
    AOPs
    , or
    Logs
    .
  2. In the dialog box, select a location to save the file and then select
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal