TRANSACTIONS tab

The TRANSACTIONS tab in the Activations view displays a log of license events, or transactions, for all machines or machines in a group. To prevent transaction log files from growing too large, FactoryTalk Updater saves transactions for four months and then discards them.
TRANSACTIONS tab columns
Column
Description
Time
The date and time the transaction occurred.
Activity
The type of transaction; for example, a license return, borrow, check out, rehost, or get.
Machine Name
The name of the machine that carried out the transaction.
Username
The user who conducted the transaction.
Feature Name
The executable file for the licensed Rockwell Automation software application; for example, RS5000.exe.
Product
The name of the licensed Rockwell Automation software application.
Serial Number
The serial number of the licensed Rockwell Automation software application.
Quantity
The number of licenses included in the transaction.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal