System requirements

Hardware requirements

FactoryTalk Updater does not have any specific hardware requirements. It runs on any hardware platform that supports the required software, either locally or on a virtual machine.
Rockwell Automation recommends at least 80 MB of available drive space for FactoryTalk Updater.

Software requirements

  • FactoryTalk Updater runs on these Windows® operating systems:
    • Windows
      10 Professional Edition 64-bit
    • Windows
      10 Enterprise 64-bit
    • Windows
      10 Enterprise 2019 LTSC 64-bit (v1809)
    • Windows
      10 Enterprise 2021 LTSC 64-bit (21H2)
    • Windows
      11 Enterprise (Recommended OS)
    • Windows
      11 Professional 64-bit
    • Windows Server®
      2019 Standard
    • Windows Server
      2019 Datacenter
    • Windows Server
      2022 Standard
    • Windows Server
      2022 Datacenter (Recommended OS)
    • Windows Server
      2025 Standard
    • Windows Server
      2025 Datacenter (Recommended OS)
  • Internet browsers:
    • Microsoft® Edge™
    • FactoryTalk Updater web client: Google® Chrome™ browser
    • FactoryTalk Updater web client: Mozilla® Firefox®
  • Installing FactoryTalk Updater installs the following software if it is not already installed:
    • .NET Framework 4.8
    • Rockwell Software Windows Firewall Configuration Utility v1.00.19
    • Microsoft .NET Hosting v8.0.18
    • IIS URL Rewrite Module v7.2.1993
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal