Local Log stops logging new messages
Possible cause and solution:
- Log file has reached its maximum file sizeIf the Local Log has been set todo not overwrite events, when the maximum file size is reached, new messages routed to the log are discarded.To resolve this situation, run theDiagnostics Setupeditor and clear the log file manually.
- Local Log destination path has been changedIf the default destination for theLocal Log Logging pathhas been changed, reboot the computer so that the new file location is used.
Provide Feedback