Some fields are not being logged to the ODBC database

Some
FactoryTalk
products use additional database fields that are not included in the ODBC table format. These additional fields cannot be logged to the ODBC database destination. Even if you create the additional fields in the database, nothing will be logged to them. The additional information logged by a
FactoryTalk
product will, however, appear in the Diagnostics local log on the computer where the product is installed. See documentation for the products you are using to determine whether they use additional fields.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal