Audit messages are not being logged

Possible cause and solution:
  • The system-wide audit policy
    Audit changes to configuration and control system
    policy is disabled. If the system policy is disabled, then FactoryTalk Diagnostics ignores audit messages generated by FactoryTalk components and FactoryTalk products and does not route them for logging even if logging destinations are configured for
    Audit messages
    on the
    Message Routing
    tab.
    Use
    FactoryTalk Administration Console
    to enable the audit policy.
    1. In
      Explorer
      , expand
      System > Policies > System Policies
      , and open
      Audit Policy
      .
    2. In
      Audit Policy Properties
      ,
      Audit changes to configuration and control system
      , select
      Enabled
      .
  • Audit messages are not logged to the ODBC database destination, regardless of whether the
    Audit changes to configuration and control system
    policy is enabled or disabled. To log audit messages to a central database, you must use
    RSMACC™
    or
    FactoryTalk AssetCentre
    software.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal