Identify the installed version of the FactoryTalk platform

Identifying the installed version of the
FactoryTalk
platform might be necessary when troubleshooting issues in the system.
To identify the installed version of the
FactoryTalk
platform
  1. Open the
    Windows
    Control Panel
    .
  2. Select
    Programs
    >
    Programs and Features.
  3. In the list of installed programs, either
    FactoryTalk Automation Platform
    or
    FactoryTalk Services Platform
    appears, with the version number shown beside it.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal