To configure the Windows Firewall
- ClickStart > Control Panel >.WindowsFirewall
- ClickAllow an app or feature through Windows Defender Firewall.
- ClickAllow another app.
- To add the database engine service:
- In theAdd an appdialog box, clickBrowse,and then go to C:\Program Files\Microsoft SQL Server\<Your SQL Server Instance Name>\MSSQL\Binn\sqlservr.exe.
- ClickOpen.
- ClickAdd.
- To add the browser service:
- In theAdd an appdialog box, clickBrowse, and then go to C:\Program Files (x86)\Microsoft SQL Server\90\Shared\sqlbrowser.exe.
- ClickOpen.
- ClickAdd.
- ClickOK.
Provide Feedback