Create a certificate signing request
FactoryTalk Linx
OPC UA Connector supports creating a Certificate Signing Request (CSR) to obtain a new certificate from an external signing authority as the Outgoing Certificate.
TIP:
Use
Manage Access
to limit access to security certificate management operations to administrators or individuals. This function is only available to Administrator.To create a certificate signing request
- InFactoryTalk Linx OPC UA Connector, selectCertificate Management.
- OnCertificate Management, selectOutgoing Certificate, and then selectCreate CSR.
- InCreate Certificate Signing Request, enter the information, and then selectOK.
- Select a location to save the CSR file, and then selectOK.
- Send the CSR file to an external signing authority for signing, and then assign the signed certificate to the OPC UA Connector onOutgoing Certificate.IMPORTANT:To ensure the automatic discovery of OPC UA servers functions properly, after the CSR file is signed and imported, import the root certificate toC:\ProgramData\OPC Foundation\UA\pki\trusted\cert.
Provide Feedback