OPC UA Server URL configuration
When
FactoryTalk Linx
OPC
UA Connector and the OPC
UA Server are in the same network environment, the OPC
UA Server must use a consistent host representation, either the host name or the IP address, across the Discovery URL and Endpoint URL.When
FactoryTalk Linx
OPC
UA Connector and the OPC
UA Server are in different network environments, the OPC
UA Server must exclusively use the IP address representation in the Discovery URL and Endpoint URL, and FactoryTalk Linx
OPC
UA Connector must also configure the OPC
UA Server Endpoint URL using the IP address representation.Provide Feedback