Share a FactoryTalk Linx driver with RSLinx Classic
The Serial-DF1 (RS232 DF1 devices) and 1784-PKTX drivers are configured in
FactoryTalk Linx
. Therefore, if you already have one of these drivers configured in RSLinx Classic
, you must delete it from RSLinx Classic
before performing the procedure below.
TIP:
This procedure describes the steps used to share a Serial-DF1 driver. However, it is also valid for sharing a 1784-PKTX driver.
To share a
FactoryTalk Linx
driver with RSLinx Classic
- Start eitheror theFactoryTalk View Studioand click theFactoryTalk Administration ConsoleCommunicationstab.
- On the communications tree, right-click the Ethernet driver (EtherNet, EtherNet), and then clickProperties.The Ethernet Properties dialog box opens.
- Click theAdvancedtab, and then selectListen on Ethernet/IP Encapsulation Portusing the check box. ClickOK.
- If you do not already have a Serial-DF1 driver inFactoryTalk Linx, then right-clickFactoryTalk Linxand clickAdd Driver, and select theSerial-DF1Serial-DF1driver from the list.TheSerial-DF1 Driver Propertiesdialog box opens.
- Click theGeneraltab, selectUse Auto-configuration. ClickOK.When you add a 1784-PKTX driver, theorDH+Driver PropertiesDH485 Driver Propertiesdialog box opens. Verify the information in the dialog box fields is correct, and clickOK.
- StartRSLinx Classic, and clickCommunications > Configure Drivers.TheConfigure Driversdialog box opens.
- From theAvailable Driver Typeslist, clickRemote Devices via Linx Gateway,and then clickAdd New.
- In theAdd New RSLinx Classic Driverdialog box, enter a driver name or use the default name. ClickOK. TheConfigure Remote Devices via Linx Gatewaydialog box opens.
- ClickBrowseto refresh the list of drivers. From theServer Namelist, select your computer name to display a list of drivers to which you can connect.
- From theRemote driver namelist, click theSerial-DF1 driver, and clickOK.TIP:When usingRSLogix, select the remote driver (for example, TCP-1) instead of the direct Serial-DF1 (for example, AB_DF1-1).
- ClickCloseto close theAdd Newdialog box.RSLinx ClassicDriver
You now have connectivity for both
FactoryTalk Linx
and RSLinx Classic
clients; the FactoryTalk Linx
driver appears in RSLinx Classic
.If, after completing this procedure, your local workstation is not displayed, restart the host computer.
Provide Feedback