Automatically upload and register a device description file
The EDS / Device Description Auto Upload function enables the to automatically upload and register device description files for a selected node and its child nodes. For an online device whose device description file is not registered, the system detects whether there is a device description file within the device's firmware. If there is a device description file found, the system automatically uploads it from the device and registers it on the current computer. With the EDS / Device Description Auto Upload function, you can register several device description files at a time.
FactoryTalk Linx
Network BrowserTo automatically upload and register a device description file
- Turn on the device description file auto-upload button
in the .FactoryTalk LinxNetwork Browser
TIP:This enables the automatic upload and registration function. By default, the function is disabled. - In the communication tree of the, double-click (or click the ">" sign beside) a node to expand and view its child devices.FactoryTalk LinxNetwork Browser
The system automatically browses the selected node and its child devices. If an unregistered online device is found, and it has a device description file within its firmware, the system automatically uploads and registers the device description file on your computer. A progress circle shows beside the unregistered device indicating the EDS / Device Description auto upload status.
Provide Feedback