Use FactoryTalk Linx Configuration Import Export Tool with command-line operation
FactoryTalk Linx
Configuration Import Export Tool- Import, export, or delete shortcuts and drivers.
- Add, update, and delete drivers.
- Browse devices to ensure that communications to a device will function when requested.
The final operation results can be checked in the
Log
file stored in the Windows Temp folder.Before using the commands to do the operations mentioned above, a user should be granted the user permission to export or import
FactoryTalk Linx
configurations.Provide Feedback