How do I change the slot number of an ENB/CNB?
The term Address is used in backplane-related configuration dialogs when what is being referred to is a slot number. The generic term Address was chosen because it provides the same appearance for all devices, backplanes, and chassis property pages. Keep in mind that a slot number is actually a backplane address.
To change the slot number of an ENB/CNB, right-click the chassis, and click
Properties.
Change the Address
field in the Properties
dialog box, click OK
and close the dialog box.Provide Feedback