Configure Remote I/O (RIO)
Use the following procedure to configure a remote I/O (RIO) scanner. This is an overview of the steps.
To configure a remote I/O scanner
- Right-clickthe RIO scanner and then clickAdd Rackto display theRack Propertiesdialog box.Note that adding a rack also adds a group to the tree. Set theRack#,Module Grouping, andAccesscontrols.When you are finished adding module groupings, clickOKto close the Rack Properties dialog box.
- Below the group that was added, right-clickInputsand/orOutputsand selectAdd Aliasto display theAlias Propertiesdialog box.
- Set theName(or accept the default name),Type,Start Address,Bit,Length,Address, andInitial Valuefields.
- ClickOverlapsto determine if any overlapping aliases exist.
- ClickApplyto save the alias to the configuration and add the next available alias to edit.
- When you are finished adding aliases, clickOKto close theAlias Propertiesdialog box.
- Right-click theRIO scannerand selectAdd Block Transferto display theBlock Transfer Propertiesdialog box.
- Set theBT #,Rack,Group/Slot,Type, andSizefields.
- ClickApplyto save the block transfer to the configuration and add the next available block transfer to edit.
- When you are finished adding block transfer definitions, clickOKto close theBlock Transfer Propertiesdialog box.
- If you wish to import a file to replace the current configuration, right-click the RIO scanner and clickImport.
- Right-click the RIO scanner and clickSave.
Provide Feedback