Add a FactoryTalk Linx data server (local)
Follow this procedure to add a
FactoryTalk Linx
data server to an application.To add a
FactoryTalk Linx
server- In theExplorerwindow, position the cursor in the area or application where you want to add theFactoryTalk Linxserver.
- Right-click the area or application icon, selectAdd New Server > Rockwell Automation Device Server (.FactoryTalk Linx)
- In thetabs, set the server properties.FactoryTalk LinxServer Properties
- ClickOKto save your changes.
- To modify the properties of aFactoryTalk Linxserver, right-click theFactoryTalk Linxserver icon, and selectProperties.
- In thetabs, change the information as required, and clickFactoryTalk LinxServer PropertiesOK.TIP:You cannot set up a redundantFactoryTalk Linxserver for a local orFactoryTalk View MEapplication.
Provide Feedback