Add Device Selection dialog box

How do I access the dialog box?
From the
Application
tab, double-click
Communication Setup
, right-click the desired driver, and then click
Add Device
.
Use the
Add Device Selection
dialog box to:
  • Add a device from the
    Available Devices
    list
  • Add a device as a
    GenericDevice, Generic Device From EDS File
    with the device description file of the device
  • Browse to the desired device description File
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal