Severity Settings Properties - Policy Settings tab
How do I open the Severity Settings Properties dialog box?
- In theFactoryTalk Administration ConsoleorFactoryTalk View StudioExplorer window, expandSystem > Policies > System Policies > FactoryTalk Alarms and Events.
- Double-clickSeverity Settings.
The
Policy Settings
tab in the Severity Settings Properties
dialog box is where you specify and apply severity settings to: - Controller status alarms generated byFactoryTalk Linx.
- Tracking events that are logged when an operator interacts with alarms.
To change severity settings for individual alarms, use the
Logix Designer
application for device-based alarms, the Alarm and Event Setup editor on the Tag Alarm and Event server for tag-based alarms, or the FactoryTalk Linx
OPC UA Connector for OPC UA alarms.Default severity settings
The following table lists the set of pre-defined events and default severity values.
FactoryTalk Linx Events | ||
Controller status alarm | Sets the severity for controller status alarms that are generated by the Rockwell Automation Device Server (FactoryTalk Linx ). | 800 |
Tracking Events | ||
Operator actions | Sets the severity for the tracking events that are logged when an operator acknowledges, resets, enables, disables, suppresses, or unsuppresses an alarm. | 100 |
To change a severity value
- To change a severity value, click in the appropriate row, and then click the arrow that appears beside the current severity value. Type a severity value or use the up and down arrow keys to change the value.
To group severity ranges into priority categories
- To make it easier to filter and sort events and distinguish among levels of urgency, the severity values of 1 to 1000 are grouped into four ranges. Each range is associated with a priority category: Urgent, High, Medium, and Low. The System Settings Properties dialog is used to set the severity ranges associated with each priority category.
Provide Feedback