Service Settings Properties - Policy Settings tab
How do I open the Service Settings Properties dialog box?
- In the FactoryTalk Administration Console or FactoryTalk View StudioExplorerwindow, expandSystem > Policies > System Policies > FactoryTalk Alarms and Events.
- Double-clickService Settings.
Use the
Policy Settings
tab in the Service Settings Properties
dialog box to change the default port of two alarm web services. The web services make alarms and events information available on the FactoryTalk System Status Portal.It is highly unlikely that you need to change these settings. Change these settings only if the default ports are in use by other applications to avoid port conflict.
The following table provides descriptions of these settings.
Setting | Description |
|---|---|
Alarm Web Data Provider Service | Specifies the communication port to access the Alarm Web Data Provider Service. The default port is 21027. The Alarm Web Data Provider Service provides access to alarms and events data providers for web-based applications. |
Alarm Web Service | Specifies the communication port to access the Alarm Web Service. The default port is 7150. The Alarm Web Service is used by web-based applications for alarms and events data. |
Provide Feedback