Use the Automatic Diagnostic Event Summary at runtime

At runtime, an operator can use the Automatic Diagnostic Event Summary to suppress, unsuppress, filter, and sort events.
At design time, the Automatic Diagnostic Event Summary can be configured to only contain selected toolbar buttons.
Use the following keyboard shortcuts to operate the Automatic Diagnostic Event Summary without a mouse at runtime.
Use this key
To do this
Home
Select the first item in the event list.
End
Select the last item in the event list.
Up arrow key
Select the previous event in the event list.
Down arrow key
Select the next event in the event list.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal