Configure appearance of the Alarm Source Browser
The
Alarm Source Browser
is divided into two panes. The left pane shows the areas from which you can select alarm sources. The right pane shows the alarm sources in the selected area.To configure the appearance of the Alarm Source Browser
- To display more of either pane, drag the bar between the two panes to the left or right.
- To sort the columns in the alarm source list, click a column heading. To reverse the sort order, click the column heading again.
- To resize the columns, drag the column headings.
- To fit the width of a column to its widest entry, double-click between two column headings.
Provide Feedback