Display server names for alarm sources
By default, the Alarm Source Browser shows only the names of alarm sources. For alarm sources with similar names, display the corresponding server names to help identify the correct source.
To display the server names for alarm sources
- Right-click anywhere in the alarm source list, and then clickShow Server Names.
Provide Feedback