Add or remove alarm sources
Add or remove alarms sources to define the origin of the alarms and events monitored.
To add or remove alarm sources
- Click an alarm source in the list. To choose multiple alarm sources from the list, do one of the following:
- To select consecutive items, click the first item, press and hold theShiftkey, and then click the last item you want to select.
- To select items that are not consecutive, click the first item, press and hold theCtrlkey, and then click the other items you want to select.
- Click theAdd selected alarm sources to selection list
button to add the selected alarm sources to the Selected alarm sourceslist at the bottom of theAlarm Source Browser. - To remove an alarm source from theSelected alarm sourceslist, click the alarm source or select multiple alarm sources, and then clickRemove.
- To remove all alarm sources from the list, clickRemove All.
Provide Feedback