Subscribe to events based on source (Summary)
Event sources can be areas, servers, or groups from which to monitor alarms. When specifying the event sources that the specific alarms subscribe to, browse the area and provide the alarm names to monitor.
To subscribe to events based on source
- Open FactoryTalk View Studio.
- Open the display that includes the Alarm and Event Summary object.
- Right-click the Alarm and Event Summary object and then clickProperties.
- Click theEvent Subscriptionstab.
- In theEvent subscriptionlist, select a subscription.
- Under theEvent sourceslist, clickBrowse.
- In theAlarm Source Browser, select the area that contains the alarms you want to monitor in the list on the left.
- Double-click the alarms in the list on the right to add them to theSelected alarm sourceslist.
- ClickOK.
- Under theEvent sourceslist, clickAddand type the area name.TIP:If you subscribe to specific alarms and you configured theScopeslist, verify that theScopeslist includes the areas that contains those alarms.
- PressEnter. You cannot subscribe to the same alarm more than once.TIP:To change the name of an alarm, click the alarm name, clickEdit, type a new alarm name, and then pressEnter.To remove an alarm, click the alarm name, and then clickRemove.
Provide Feedback