Different event types in the Alarm and Event viewer
Different types of events are treated differently in the Alarm and Event viewer.
The following list describes the events and provide an example of the event:
- Tracking-related eventAn event that tracks changes made to the system over time. Examples: an event describing the acknowledgment of an alarm by an operator, or the modification of a tag value by an operator.
- Condition-related eventAn event associated with a change in the state of an alarm. For example, a condition-related event is triggered when an alarm condition changes to In Alarm, Acknowledged, Return to Normal, or Disabled.
- Simple eventsAny event describing a simple occurrence in the system. For example, failure in accessing a computer or device.
Provide Feedback