Configure the Alarm and Event Log Viewer
At design time the Alarm and Event Log Viewer can be configured using the tabs in the
Alarm and Event Log Viewer Properties
dialog box. Configuring these properties changes how information is displayed and how the operator can interact with the information in the Alarm and Event Log Viewer at runtime.This dialog is opened from
FactoryTalk View
Studio by right-clicking the Alarm and Event Log Viewer object and then clicking Properties
.Provide Feedback