Configure the Alarm and Event Banner
The appearance of the Alarm and Event Banner can be customized by configuring the Alarm and Event Banner Properties settings. Each area of the banner has a properties tab that contains the settings that apply to that area.
Using these settings you can change which alarm and event servers are subscribed to by the banner, add, remove and format columns and rows in the alarm list, change the sort order of the alarm lists, as well as change the colors, font, and button size of the items on the banner.
Provide Feedback