Columns in the Alarm and Event Banner
The data fields in the Alarm and Event Banner alarm list are organized into columns and represent the following alarm and event information. The columns selected at design time are displayed in the Alarm and Event Banner at runtime.
The following tables describes the information contained in the columns:
Column | Description |
|---|---|
Priority | The urgency of the event:
|
Severity | The severity of the event. This is a value in the range of 1 (lowest severity) through 1000 (highest severity). |
Alarm State | The state of the alarm condition:
|
Event Time | The time at which the alarm condition or sub-condition changed into the currently displayed state. The time can include seconds, milliseconds, or microseconds depending on the timestamp type selected in the Show seconds for all timestamps drop-down list box. |
In Alarm Time | The time at which the alarm condition changed state from Normal to In Alarm. The time can include seconds, milliseconds, or microseconds depending on the timestamp type selected in the Show seconds for all timestamps drop-down list box. |
Acknowledge Time | The time at which the alarm condition became acknowledged. The time can include seconds, milliseconds, or microseconds depending on the timestamp type selected in the Show seconds for all timestamps drop-down list box. |
Out of Alarm Time | The time at which the alarm condition changed into the Normal state. Internally FactoryTalk Alarms and Events normalizes time values to Greenwich Mean Time (GMT). Objects such as the FactoryTalk Alarm and Event Banner then convert the time values to the local time zone of the computer where the object is running. For example, the Event Time displayed on computers in different time zones will differ by the number of hours between their time zones. Also, the display format of date and time values are controlled by the Windows Regional Settings in the Control Panel on the computer where the FactoryTalk Alarm and Event Banner is running. |
Area | The FactoryTalk Directory path to the area in which the event occurred, in the format /Area1/SubArea1/... . For example: /Line1/MixingTank . |
Server Name | The name of the server that generated the event. For example: Packaging Server. |
Group | The name of the group associated with the alarm, in the format Group1.SubGroup1 . |
Alarm Name | The full qualified name of the alarm without the area path and server name. For example, [Line1Controller]Program:Line1Program.MixingTank1 . |
Alarm Short Name | The short name of the alarm. For example, MixingTank1 . |
Condition Name | A name that describes the alarm condition. Condition names vary by event category. For example,
|
Message | The text that describes the event. |
Alarm Count | The number of times the alarm condition has gone In Alarm. The alarm count can be reset from the Alarm Details dialog box which is accessible from the Alarm and Event Summary and the Alarm Status Explorer . |
Alarm Class | A classification string associated with an alarm when it is defined. The Alarm Class provides a user defined string that can be used for filtering and sorting alarms. |
Provide Feedback
Low
Medium
High
Urgent
In Alarm and Unacknowledged
In Alarm and Acknowledged
Normal and Unacknowledged