About the Alarm and Event Banner Object Model
Use the object model to programmatically control what an operator can see and do in the FactoryTalk Alarm and Event Banner object. The object model allows you to:
- Control access to column values for the currently-selected row.
- Produce events when the user clicks or double-clicks a row.
- Expose or conceal operations that affect the alarms and events system:
- Acknowledging alarms.
- Silencing or sounding the alarm bell.
Provide Feedback