Add and remove user-computer pairs
Security for
FactoryTalk
resources is always tied to users or groups of users, the actions the users perform, for example, read, write, and so on, and the computers, or groups of computers where the users work.This ensures that only authorized personnel can perform actions on the equipment and resources in the system from appropriate locations, for example, computers located within line of sight of equipment.
Available options are:
Provide Feedback