Restore (Security Authority Identifier)
How do I open Restore?
- In theExplorerwindow, verify that the applications located in the directory that you are restoring into are not currently expanded or being used by some other product or component.
- Right-clickNetworkorLocal,and clickRestore.
Setting | Description |
|---|---|
Archive name | The name of the backup archive file to be restored. By default, the archive name is ApplicationName.bak file. |
Directory type | Identifies the type of information held within the backup archive file.
|
Application(s) | The name of the application or applications held in the backup archive file. |
Restore directory contents only | Restores applications, users, computers, groups, passwords, policies, and security settings. The security authority identifier is not restored. |
Restore security authority identifier only | Only restores the security authority identifier. Applications, users, computers, groups, passwords, policies, and security settings are not restored. Back up your directory and remove the old bindings from all controllers and controller projects before continuing. Back up the directory with the new identifier after the restore process is completed. |
FactoryTalk Directory configuration | Restores applications, users, computers, groups, passwords, policies, and security settings. This option is only available when Restore directory contents is selected. |
FactoryTalk Linx configuration | Restores shortcut and driver configurations of FactoryTalk Linx .Only FactoryTalk Linx configurations exist on the local PC can be restored. Refer to Restore FactoryTalk Linx configuration to find how to restore a distributed system. |
FactoryTalk Linx Gateway configuration | Restores server configuration, UA Server Endpoint settings, Advanced Settings, and UA Tag List configuration in FactoryTalk Linx Gateway . |
Provide Feedback