Restore an earlier system after upgrading FactoryTalk platform software

An archive file created using
FactoryTalk Services Platform
6.10 cannot be restored on a computer running an earlier version of
FactoryTalk Services Platform
. You must use the archive file created before you installed
FactoryTalk Services Platform
6.10 to revert to a previous version.
Before restoring to an earlier system, keep the following in mind:
  • Following the instructions in this topic overwrites all data in the
    FactoryTalk Directory
    and returns it to the state it was in before upgraded. For example, any applications, security settings, or system policies will be lost. If you want to keep any of this data, back up the network directory and local directory now.
  • When reverting from
    FactoryTalk Services Platform
    2.10 (CPR 9) or later to an earlier version of the platform, you must restore backup archives for both the network directory and the local directory, even if you plan to use only one of the directories.
  • If you upgraded to
    FactoryTalk Services Platform
    version 2.10 (CPR 9) or later, backups of the earlier version of the local directory and network directory were automatically created. You can use those backups to revert to an earlier version.
  • Do not restore an archive file created with
    FactoryTalk Services Platform
    2.10 (CPR 9) or later into a
    FactoryTalk Directory
    that is running
    FactoryTalk Services Platform
    2.00 (CPR 7). This is not supported and may have unexpected results.
  • As part of re-installing an earlier version of
    FactoryTalk Services Platform
    or
    FactoryTalk Automation Platform
    , you will need to enter the
    FactoryTalk
    administrator user name and passwords that were saved in the backup archive of the
    FactoryTalk Directory
    .
To restore an earlier system after upgrading
FactoryTalk
platform software
  1. Uninstall all
    FactoryTalk
    software products that are incompatible with the version of the
    FactoryTalk
    platform you plan to use.
    1. To verify the version of the
      FactoryTalk
      platform software that a product requires, see the product's installation documentation.
    2. Go to
      Control Panel > Uninstall a program
      or
      Programs and Features
      .
    3. Uninstall
      FactoryTalk Services Platform
      .
    4. Uninstall
      Windows Firewall Configuration Utility
      .
  2. Restart your computer.
  3. Delete the folders
    C:\ProgramData\Rockwell\RNAServer
    and
    C:\ProgramData\Rockwell\RNAClient
    .
  4. Install the version of the
    FactoryTalk
    platform software you plan to use. If the version is 2.10 (CPR 9) or later, skip to the next step after installation. If the version is 2.00 (CPR 7), do the following:
    • On the
      Overview
      page of the
      FactoryTalk Directory
      Configuration Wizard, select both
      FactoryTalk Network Directory
      and
      FactoryTalk Local Directory
      and then select
      Next
      .
    • If prompted, enter a
      FactoryTalk
      administrator user name and password for each directory.
  5. Install earlier versions of all software products that are compatible with the version of the
    FactoryTalk
    platform software you plan to use. To verify the version of the
    FactoryTalk
    platform software that a product requires, see the product's installation documentation.
  6. Run
    FactoryTalk Administration Console
    and log on to the Local Directory. In
    Explorer
    , right-click the
    Local
    icon and then restore a local backup archive created with the earlier version of the
    FactoryTalk
    platform software.
  7. Select
    File
    >
    Log Off
    to log off the local directory, and then log on to the network directory. Right-click the
    Network
    icon and then restore a network backup archive created with the earlier version of the
    FactoryTalk
    platform software.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal