Restore (System folder)
How do I open Restore?
- In theExplorerwindow, verify that the applications located in the directory that you are restoring into are not currently expanded or being used by some other product or component.
- Right-clickNetworkorLocal,and clickRestore.
After selecting a system-only archive file,
Restore
displays the archive name and the archive type.Restoring a System folder moves the following system-wide settings from one
FactoryTalk Directory
to another:- The list of user, computer, and group accounts
- Action groups
- Passwords
- Policy settings
- Security settings
- Alarm and event database definitions
Review the following settings before selecting
Finish
to restore a System folder. Setting | Description |
|---|---|
Archive name | The name of the backup archive file to restore. |
Directory type | Identifies the type of information held within the backup archive file. System Only - Restoring the System folder overwrites all user and computer accounts and groups, passwords, policy settings, and security settings for all applications in the FactoryTalk Directory . |
Application(s) | Archive does not contain any application - Confirms that applications are not included in the backup archive to restore. |
System Directory configuration | This option is selected by default to restore the entire System folder. Restoring the System folder overwrites all user and computer accounts and groups, passwords, policy settings, and security settings for all applications in the FactoryTalk Directory . |
Provide Feedback