Summary
How do I open Summary?
Click
OK
in the second wizard screen--Reconfigure a Network Directory
or Reconfigure a Local Directory
. When the FactoryTalk Directory Configuration Wizar finishes,
Summary
shows a list of what the FactoryTalk Directory
Configuration Wizard did, together with any errors that might have occurred. These errors are also logged to FactoryTalk Diagnostics
and can be reviewed using the FactoryTalk Diagnostics
Viewer.If an error occurred while running the
FactoryTalk Directory
Configuration Wizard, review the errors shown in Summary
, and refer to the list of common errors below. After resolving the likely problems, run the wizard again. Common causes for errors include:
- Insufficient disk space. Clear some disk space and then run the wizard again.
- You are not logged on as an administrator. You must be logged on as an administrator to run theFactoryTalk DirectoryConfiguration Wizard. To run the wizard because an error occurred during installation for the first time on a computer, you must be logged on as aWindowslocal administrator.
- The. This error applies to only theFactoryTalkDirectory is in read-only modeFactoryTalknetwork directory. This error appears as a warning when your computer cannot communicate with theFactoryTalknetwork directory server, or if the network connection is lost while configuring the directory. Make sure both your computer and theFactoryTalknetwork directory are connected to the network. You donotneed to run the wizard again after reconnecting to theFactoryTalknetwork directory server.
- You are attempting to configure the. You cannot use Remote Desktop Services to configure aFactoryTalk Directoryfrom a remote computerFactoryTalk Directory. You must configure aFactoryTalklocal directory at the local computer. You must configure aFactoryTalknetwork directory at the computer that is theFactoryTalknetwork directory server.
Provide Feedback