Manage servers

A
FactoryTalk Directory
holds any number of data servers, device servers, alarm and event servers, and HMI servers. Add a server to an application or an area to create a link between the server and the
FactoryTalk Directory
. Each area can have one HMI server.
Add the following servers to either an application or an area:
After adding a server:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal