Back up a Security Authority identifier
Each
FactoryTalk Directory
has a unique Security Authority identifier generated during installation. Back up a Security Authority identifier to save the identifier in case of disaster.Secure controller projects and controllers running secure projects can only be accessed when the
FactoryTalk Directory
Security Authority identifier matches the identifier saved in the project. This prevents unauthorized access to a controller or controller project if moved or copied to a different FactoryTalk Directory
.Prerequisites
- Obtain the following permissions fromSystem > System Policies > User Rights Assignment:
To back up the security authority identifier
- InFactoryTalk Administration Console, selectTools >.FactoryTalkSecurity Authority Identifier
- InModify Security Authority Identifier, selectBackup.
- (optional) InBackup, set the backup archive options:
- Specify archive name:Type the name for the backup archive.
- Specify archive location:Type or browse to a path for the backup archive.
- Specify backup contents:
- Selectto back up the entireFactoryTalk DirectoryconfigurationFactoryTalk Directory.
- Selectto back up shortcut and driver configurations.FactoryTalk Linxconfiguration
- Selectto back up server configuration, UA Server Endpoint settings, Advanced Settings, and UA Tag List configuration inFactoryTalk Linx GatewayconfigurationFactoryTalk Linx Gateway.
- Encrypt file contents:Select to protect the backup archive with a passphrase, then enter the passphrase into the passphrase fields. Clear to save the backup archive as plain text.
- SelectOK.
- (optional) If prompted, selectYesto overwrite the existing backup archive.
- In the confirmation window, selectOK.IMPORTANT:FactoryTalk Services Platform6.10 applies a new encryption algorithm to the backup file for enhanced security. Backups created usingFactoryTalk Services Platform6.10 can only be restored to host computers that are also runningFactoryTalk Services Platform6.10 or later. Backups created usingFactoryTalk Services Platform2.90 or later can be restored onto host computers that are runningFactoryTalk Services Platform6.10.
Provide Feedback