Alarm dashboard
The alarm dashboard includes real-time and historical data.
The real-time alarm summary shows the number of total alarms, in alarm, unacked, shelved, suppressed, disabled, and bad alarms from a specific alarm server. The real-time data will be refreshed every 5 seconds.
The historical data will filter alarms in the recent year with a maximum of 1,000,000 and will be refreshed every 30 minutes. The summary shows the data in a period from the following charts:
- Top 10 frequent alarmsShows the most 10 frequent alarms and the Pareto chart.
- Priority distributionShows the number and ratio of alarms of each priority.
- Top 10 stale alarmsShow the top 10 alarms with the longest active state duration.
- Alarm occurrencesShows the number and priority distribution of alarms.
Provide Feedback