FactoryTalk Linx OPC UA Connector considerations-Help

FactoryTalk Linx
OPC
UA Connector supports
OPC
UA Servers with the following considerations:
  • FactoryTalk Linx
    OPC
    UA Connector can be added to applications or areas in a
    FactoryTalk
    Network Directory or a
    FactoryTalk
    Local Directory.
  • A maximum of 20
    OPC
    UA Servers can be connected to a single OPC UA Connector. To use more than 20 OPC UA Servers or to spread the system resource load across multiple host computers, add multiple
    OPC
    UA Connectors to a
    FactoryTalk
    application.
  • OPC UA Connectors and OPC UA Servers must communicate over an IPv4 network. IPv6 connectivity is not supported.
  • OPC UA Servers must communicate using the
    opc.tcp://
    protocol. Other protocols, such as
    http://
    and
    https://
    are not supported.
  • OPC UA Servers must support subscriptions with poll rates to read tags. Read requests are not supported.
  • OPC UA Servers that impose limits on the number of items that can be incorporated into a single subscription may not work as expected. All items monitored at the same rate are added to the same subscription. If the number of items in one subscription exceeds an OPC UA Server limit, items in the subscription may fail.
  • If an established subscription is disconnected, it is retained and can be reconnected if the communication recovers within 10 minutes. If the disconnection lasts more than 10 minutes, a new connection request will be submitted for the client to establish the connection.
  • After the initial OPC UA Server connection or after refreshing tag names, there is a delay before all server tags appear in the
    FactoryTalk
    Tag Browser. The delay time is dependent on OPC UA Server specifications, network specifications, and the data model of the tags provided to the OPC UA Connector.
    To determine if the tag name upload is complete, monitor the
    @OPC_NamespaceCacheUploadCompleteStatus
    predefined diagnostic item of the OPC UA server.
    To determine if an error has occurred during the tag name upload, view
    FactoryTalk Diagnostic Log
    .
  • The OPC UA Connector performance of namespace processing and browsing is better when using the network scope than using the local scope.
  • Server names, folder names, or node ID names containing a forward slash (/) are not supported.
  • FactoryTalk OPC UA Connector uses TCP ports on the target workstation hosting the OPC UA Server to be open and accessible. Review the OPC UA Server's configuration and ensure that any TCP ports are opened and available for communications. It might be necessary to modify the workstation operating system and firewall. For more information, refer to Knowledgebase Document ID: IN40928 - Security Software Considerations to Prevent or Mitigate Impacts to Rockwell Automation Software Products.
  • FactoryTalk Linx
    OPC UA Connector new features supported by
    FactoryTalk Services Platform
    version 6.10.00 cannot be configured or used by computers running
    FactoryTalk Services Platform
    version 3.00.00 or earlier. To use these features, update
    FactoryTalk Services Platform
    on all computers hosting
    FactoryTalk Linx
    OPC UA Connectors to version 6.10.00 or later.
  • To use the redundancy capability of
    FactoryTalk Linx
    OPC UA Servers, use
    FactoryTalk Services Platform
    version 6.20.00 or later.
  • Data coming from an OPC UA Server, delivered through the OPC UA Connector, may not update even though the OPC UA Server delivers new values. The OPC UA Connector evaluates a time stamp provided with the data value to help prevent delivering data that is older than a previous value. If an OPC UA Server sends a value with a time stamp older than a previous value, the OPC UA Connector ignores it, indicating that that there may be a problem with the OPC UA Server or device. First identified in
    FactoryTalk Linx
    OPC UA Connector version 6.20.00.
  • When a variable node’s datatype is defined as a Structure (NodeId: i=22),
    FactoryTalk Linx
    OPC UA Connector will identify it as a folder instead of a data item. If you do a namespace analysis, all such tags will be identified as "folder (raw 'Structure' type (i=22) not supported)."
  • An OPC UA Server can define structures to send structure values as both encoded data containing all fields and separate values for each individual field.
    FactoryTalk Linx
    OPC UA Connector can read the values for both types, but it cannot write values to fields within the encoded data. If the value is accessed as encoded data, it is read-only, and the tags representing a structure’s fields within the encoded data are shown in FactoryTalk software with periods (".") between each structure level. If a structure value is accessed as individual fields,
    FactoryTalk Linx
    OPC UA Connector can write values to it, and the tags representing a structure’s fields are shown in FactoryTalk software with slashes ("\") between each structure level.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal