Remove columns
FactoryTalk Live Data Test Client
displays data in a grid composed of columns and rows. Some data columns can be removed from the display using the View
menu. This can be useful when horizontal space is limited.To remove columns
- From theViewmenu, selectColumns. The columns currently shown inFactoryTalk Live Data Test Clientdisplay with check marks.
- Clear a check mark column from the menu. The check mark is removed from the menu item and the column is removed from theFactoryTalk Live Data Test Clientdisplay.
Provide Feedback