Reconnect to a data source
Reconnect to a data source to select a different data server or configuration file.
IMPORTANT:
Connecting to a different server deletes all of the current groups. To save the current configuration of data items and group, save the config file.
To reconnect to a data source
- InFactoryTalk Live Data Test ClientselectFile>Reconnect.
- InInitial Connectionselect the type of data source, either:
- OPC DA Server
- Factory Talk
- Load Config File
- Specify the location of the data source to connect to.
- OPC DA Server: Select an OPC DA server from the list. In OPC DA Server Machine, select either Local or Remote. If remote, type the computer name of the remote server in the space provided.
- Factory Talk: When prompted, select theFactoryTalk Directory, eitherNetworkorLocal, and selectOK. The list of availableFactoryTalkservers appears. Expand the list as necessary to locate the data server to connect to, and selectOK.
- Load Config File: SelectBrowseto select a saved config file.
- SelectOKto switch to the new data source.
Provide Feedback