Load a config file
Load a config file to open a collection of previously saved data items and groups for monitoring. A config file is saved in XML format.
To load a config file
- Start theOPCor otherFactoryTalk-enabled server.
- To connect toFactoryTalk® Linx, start theFactoryTalk Linxdata server.
- To connect toFactoryTalk® View Site Edition (SE), start theFactoryTalk View SEorFactoryTalk View Studio, and then open an application.
- Go toRockwell Software > FactoryTalk Toolsand open.FactoryTalk Live Data Test Client
- InInitial Connection, selectLoad Config File.
- If the configuration file appears in the list, select it. Continue to step 7.
- If the configuration file does not appear in the list, selectBrowse.
- InOpen, navigate to the location where the configuration XML file is stored and select the XML file, then selectOpen.
- SelectOKto load the file:
Provide Feedback