Connect FactoryTalk Live Data Test Client to an OPC DA server
Connect
FactoryTalk Live Data Test Client
to an OPC
DA server, such as RSLinx Classic
, to monitor, read, and write data items in the data server.To connect
FactoryTalk Live Data Test Client
to an OPC
DA server- Start theOPCserver. For example, to monitor tags in anRSLinx Classicdata server, startRSLinx Classic.
- Go toRockwell Software > FactoryTalk Toolsand openFactoryTalk Live Data Test Client
- InInitial Connection, selectOPC DA Server.
- Select theOPCserver from the list of available servers. If theOPCserver is not shown, verify it is running and accessible over the network.TIP:When connecting toRSLinx Classic, always selectbecause this provides the most reliable connection.RSLinxRemote OPC Server
- InOPC DA Server machine, select either:
- LocalIf theOPCserver is located on the same computer as theFactoryTalk Live Data Test Client.
- RemoteIf theOPCserver is located on a remote computer. Type the name of the remote computer in the space provided.
- (optional) If the OPC DA Server is in a different region, inOPC DA Server Locale IDenter the locale code. Examples: English-US = 1033, Chinese-China = 2052, French-France = 1036, German-Germany = 1031.
- When finished, selectOK.
Provide Feedback