Configure features supported in the container

Configure features supported in the container

Runtime is designed as a multi-container application, which means you can use Docker Compose to run it.
Set the environment variables in the .env file according to the environment variables that best suit your needs before executing the Docker Compose command. The .env file should look like this:
SETUPHOSTIMAGE=factorytalkremoteaccess/setuphost RUNTIMEIMAGE=factorytalkremoteaccess/runtime TAG=<version> SETUPHOSTCONTAINER=factorytalkremoteaccess-setuphost RUNTIMECONTAINER=factorytalkremoteaccess-runtime VERBOSE=false VOLUME= TZ=UTC APPARMOR_PROFILE=factorytalkremoteaccess_runtime WEB_LOGIN_PASSWORD= RDP_DISPLAY= RDP_XAUTHORITY= VPN_ADAPTERS= VPN_P2P=false
Environment variables
Variable
Definition
Note
SETUPHOST_IMAGE
Specifies the image name of the Setuphost service.
ALREADY SET
RUNTIME_IMAGE
Specifies the image name of the Runtime service.
ALREADY SET
TAG
Defines the tag for both images.
ALREADY SET
SETUPHOST_CONTAINER
Indicates the container name associated with the Setuphost service.
ALREADY SET
RUNTIME_CONTAINER
Indicates the container name associated with the Runtime service.
ALREADY SET
VERBOSE
Enables detailed output from the Setuphost in operation if set to
true
. The default value is
false
.
EDITABLE
VOLUME
Specifies the path to the volume mounted by the Runtime to store persistent data. For example,
/path/to/persistent/folder
.
SET MANDATORILY
TZ
Sets the time zone where the Runtime operates. By default, the time zone is set to
UTC
. You can change this preset time zone by modifying the
UTC
value.
EDITABLE
APPARMOR_PROFILE
Defines the AppArmor profile applied to the Runtime service. To run the container without complying with any security policies, remove this variable or set it to
unconfined
.
EDITABLE
WEB_LOGIN_PASSWORD
Protects the Web UI of the Runtime through a password. This variable is not set by default, but it is recommended to set it for security purposes. This value is entered into the Setuphost service as a secret.
EDITABLE
RDP_DISPLAY
Specifies the host display used by the Runtime to run the Remote Desktop feature. See Enable the Remote Desktop Protocol (RDP).
SET ONLY FOR RDP
RDP_XAUTHORITY
Specifies the path to the
.Xauthority
file used by the standard user that interacts with the X11 server. See Enable the Remote Desktop Protocol (RDP).
SET ONLY FOR RDP
VPN_ADAPTERS
Specifies the interfaces with which the Runtime can establish VPN connections. See Enable a VPN connection.
SET ONLY FOR RDP
VPN_P2P
Enables the Point-to-Point VPN feature in Runtime if set to
true
. The default value is
false
.
SET ONLY FOR RDP
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal