- Software components setup and installation
Data center
Security Standards
Access Servers, Database Servers and the Web API servers are hosted on Microsoft Azure.
Azure is certified for ISO/IEC 27001:2013 and other security standards and certifications.
Refer to the following pages:
FactoryTalk®
Remote Access™
FactoryTalk®
Remote Access™
- Relay Servers are dynamically discovered. Even if a node is not available, clients will automatically switch to the others.
- Relay Servers are an intermediate hop of an end-to-end encrypted channel, explained earlier. A man-in-the-middle attack scenario is not possible.
- No data is stored on Relay Servers.
Backup
SQL backups are automatically managed by Azure and geographically spread in order to minimize the possibility of data loss.
Provide Feedback