log-in-to-factorytalk-hub

Log in to
FactoryTalk® Hub

FactoryTalk® Hub
includes different cloud-based SaaS applications, displayed in the form of tiles. Log in to
FactoryTalk® Hub
to access your application.
  1. Go to FactorytalkHub.com to launch
    FactoryTalk® Hub
    .
  2. TIP: If you do not have a MyRockwellAutomation account, see Create your MyRockwellAutomation account.
    In the
    Sign in
    pane, enter the same email that you use for your MyRockwellAutomation account.
  3. Enter the same password that you use for your MyRockwellAutomation account.
    A
    Important: MFA Skip Limit Warning
    message appears.
  4. In the
    Select verification method
    pane, select a verification option, and then select
    CONTINUE
    .
    IMPORTANT: You can select a verification method other than email, such as SMS text message, or phone call. To select SMS text message or phone call, you must have entered your phone number when you created your MyRockwellAutomation account in the
    Advanced Access
    section.
  5. Enter a verification code as required in the
    Two-step verification
    pane or enter the code on the phone, depending on the verification method that you previously selected.
  6. The first time you log in to
    FactoryTalk® Hub
    , scroll to read the Rockwell Automation EULA and then select
    Accept
    .
    You are prompted to either join an existing organization or create a new one.
TIP: To learn more about the
FactoryTalk® Hub
, see FactoryTalk Hub online Help.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal