Edit Global Settings

Edit Global Settings to change the policy model name, configure certificate and ports settings, and enable or disable features.
Prerequisites
  • Log on to
    FactoryTalk Policy Manager
    as an administrator.
  • Learn about the available settings. See Global Settings.
  1. To Edit Global Settings
  2. From the navigation bar, select
    Global Settings
    .
  3. Edit fields.
    TIP: Changes are saved when you select another field or exit
    Global Settings
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal