Replace a device
Replace a device if a device that was configured has failed or must be rotated out for maintenance.
TIP:
Device replacement enables the identity and the security configuration of the
previous device to be assigned to the replacement device.
TIP:
Replacing devices configured as Redundant Chassis Pairs is not
supported. For more information, see Redundancy system.
After replacing a redundant device physically, either deploy or validate the security policy
model to verify that the device properties are correct. See Deploy a policy model and Validate a policy model.
- From the navigation bar, either:
- SelectCanvas.
- SelectZonesand then select a zone.
- SelectDevices.
- Right-click the device to replace and selectReplace Device.TIP: InZonesorDevices, you can also select the device to replace and then selectReplace Devicefrom the toolbar.
- InDeploy Configuration to Replace Deviceselect when to reset the communication ports on the device:
- To reset the ports automatically as part of the replacement process, selectDuring policy deployment.
- To reset the ports manually at a later time, selectAfter deployment. The security policy is not being enforced on the device until the ports are reset.
- Deploy the policy model to apply the security policies to the replaced device.For more information, see Policy model validation and deployment.
Provide Feedback