Disable Automatic Policy Deployment

Disable Automatic Policy Deployment by editing global settings and manually closing ports on the machine.
TIP:
The
FactoryTalk Policy Manager
installation agent opens these Windows Firewall ports:
UDP 5353
and
TCP 40014
. To operate correctly, the Automatic Policy Deployment functionality requires these ports to be open.
  1. Open
    FactoryTalk Policy Manager
    , select
    Global Settings
    and clear the
    Enable automatic device discovery and onboarding
    checkbox.
  2. Manually close the
    UDP 5353
    and
    TCP 40014
    ports on the machine.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal